This is a source sequence parameter which specifies the frequency to be generated, either directly (in MHz) or by channel number. If the radio band specified by the Band parameter is NONE, the present parameter represents the frequency in MHz; otherwise, the present parameter represents the channel number.
There is no dropdown list for this field; it is necessary to enter a suitable value, or accept the default value of 1000.